public static class FillHoleBuilder.TargetTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BY_NUMBER_OF_EDGES
Automatically target holes based on number of edges.
|
static int |
_USER_DEFINED
Fills user-defined target holes.
|
static FillHoleBuilder.TargetTypes |
BY_NUMBER_OF_EDGES
Automatically target holes based on number of edges.
|
static FillHoleBuilder.TargetTypes |
USER_DEFINED
Fills user-defined target holes.
|
Modifier and Type | Method and Description |
---|---|
static FillHoleBuilder.TargetTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FillHoleBuilder.TargetTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FillHoleBuilder.TargetTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final FillHoleBuilder.TargetTypes USER_DEFINED
public static final FillHoleBuilder.TargetTypes BY_NUMBER_OF_EDGES
public static final int _USER_DEFINED
public static final int _BY_NUMBER_OF_EDGES
public static FillHoleBuilder.TargetTypes valueOf(int value)
public static FillHoleBuilder.TargetTypes valueOf(String name)
public static FillHoleBuilder.TargetTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.