public interface TrueShadingCollection extends TaggedObjectCollection
BasePart
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
TrueShadingBuilder |
createTrueShadingBuilder(TrueShading sObj)
Creates a
TrueShadingBuilder object
if SHED is null. |
TrueShading |
findObject(String journalIdentifier)
Finds the
TrueShading with the given identifier
as recorded in a journal. |
_find_next, iterator
TrueShadingBuilder createTrueShadingBuilder(TrueShading sObj) throws NXException, RemoteException
TrueShadingBuilder
object
if SHED is null. Otherwise, a TrueShading object will be edited
sObj
- If SHED object is not null, then this object will be editedNXException
RemoteException
TrueShading findObject(String journalIdentifier) throws NXException, RemoteException
TrueShading
with the given identifier
as recorded in a journal. An object may not return the same value as its
JournalIdentifier in different versions of the software. However newer versions
of the software should find the same object when FindObject is passed older versions
of its journal identifier. In general, this method should not be used in handwritten
code and exists to support record and playback of journals.
An exception will be thrown if no object found with the given journal identifier.
journalIdentifier
- Identifier to be foundNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.