public static class StudioImageCaptureBuilder.DrawingSizeEnumType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANSIA
Use ANSI A drawing size
|
static int |
_ANSIB
Use ANSI B drawing size
|
static int |
_ANSIC
Use ANSI C drawing size
|
static int |
_ANSID
Use ANSI D drawing size
|
static int |
_ANSIE
Use ANSI E drawing size
|
static int |
_CUSTOM
Use custom defined drawing size
|
static int |
_ISOA0
Use ISO A0 drawing size
|
static int |
_ISOA1
Use ISO A1 drawing size
|
static int |
_ISOA2
Use ISO A2 drawing size
|
static int |
_ISOA3
Use ISO A3 drawing size
|
static int |
_ISOA4
Use ISO A4 drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ANSIA
Use ANSI A drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ANSIB
Use ANSI B drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ANSIC
Use ANSI C drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ANSID
Use ANSI D drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ANSIE
Use ANSI E drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
CUSTOM
Use custom defined drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ISOA0
Use ISO A0 drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ISOA1
Use ISO A1 drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ISOA2
Use ISO A2 drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ISOA3
Use ISO A3 drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
ISOA4
Use ISO A4 drawing size
|
Modifier and Type | Method and Description |
---|---|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioImageCaptureBuilder.DrawingSizeEnumType[] |
values()
Returns an array that contains the values for this enum.
|
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ISOA4
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ISOA3
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ISOA2
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ISOA1
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ISOA0
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ANSIA
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ANSIB
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ANSIC
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ANSID
public static final StudioImageCaptureBuilder.DrawingSizeEnumType ANSIE
public static final StudioImageCaptureBuilder.DrawingSizeEnumType CUSTOM
public static final int _ISOA4
public static final int _ISOA3
public static final int _ISOA2
public static final int _ISOA1
public static final int _ISOA0
public static final int _ANSIA
public static final int _ANSIB
public static final int _ANSIC
public static final int _ANSID
public static final int _ANSIE
public static final int _CUSTOM
public static StudioImageCaptureBuilder.DrawingSizeEnumType valueOf(int value)
public static StudioImageCaptureBuilder.DrawingSizeEnumType valueOf(String name)
public static StudioImageCaptureBuilder.DrawingSizeEnumType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.