public static class RayTracedStudioEditorBuilder.StationaryAntialiasingType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LOW
Coarse antialiasing performed when dynamic interaction stops
|
static int |
_MEDIUM
Good antialiasing performed when dynamic interaction stops
|
static int |
_NONE
No antialiasing performed to provide quick, preview of ray traced display when dynamic interaction stops
|
static RayTracedStudioEditorBuilder.StationaryAntialiasingType |
LOW
Coarse antialiasing performed when dynamic interaction stops
|
static RayTracedStudioEditorBuilder.StationaryAntialiasingType |
MEDIUM
Good antialiasing performed when dynamic interaction stops
|
static RayTracedStudioEditorBuilder.StationaryAntialiasingType |
NONE
No antialiasing performed to provide quick, preview of ray traced display when dynamic interaction stops
|
Modifier and Type | Method and Description |
---|---|
static RayTracedStudioEditorBuilder.StationaryAntialiasingType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RayTracedStudioEditorBuilder.StationaryAntialiasingType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RayTracedStudioEditorBuilder.StationaryAntialiasingType[] |
values()
Returns an array that contains the values for this enum.
|
public static final RayTracedStudioEditorBuilder.StationaryAntialiasingType MEDIUM
public static final RayTracedStudioEditorBuilder.StationaryAntialiasingType LOW
public static final RayTracedStudioEditorBuilder.StationaryAntialiasingType NONE
public static final int _MEDIUM
public static final int _LOW
public static final int _NONE
public static RayTracedStudioEditorBuilder.StationaryAntialiasingType valueOf(int value)
public static RayTracedStudioEditorBuilder.StationaryAntialiasingType valueOf(String name)
public static RayTracedStudioEditorBuilder.StationaryAntialiasingType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.