public interface PointCloudCollection extends TaggedObjectCollection
BasePart
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
PointCloudBuilder |
createPointCloudBuilder(PointCloud referencePointCloud)
Creates a
PointCloudBuilder object
used to build a point cloud. |
PointCloud |
findObject(String journalIdentifier)
Finds the
PointCloud with the given
identifier as recorded in a journal. |
_find_next, iterator
PointCloud findObject(String journalIdentifier) throws NXException, RemoteException
PointCloud
with the given
identifier as recorded in a journal. An object may not return the same
value as its JournalIdentifier in different versions of the software.
However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In
general, this method should not be used in handwritten code and exists
to support record and playback of journals.
journalIdentifier
- Identifier to be foundNXException
RemoteException
PointCloudBuilder createPointCloudBuilder(PointCloud referencePointCloud) throws NXException, RemoteException
PointCloudBuilder
object
used to build a point cloud.
If the referencePointCloud is not null, the referencePointCloud object will be edited.
referencePointCloud
- If referencePointCloud is not null,
this object will be editedNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.