public static class ImageBaseBuilder.InsertionPoint extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEFAULT
default insertion point type
|
static int |
_USER_DEFINED
user defined insertion point type
|
static ImageBaseBuilder.InsertionPoint |
DEFAULT
default insertion point type
|
static ImageBaseBuilder.InsertionPoint |
USER_DEFINED
user defined insertion point type
|
Modifier and Type | Method and Description |
---|---|
static ImageBaseBuilder.InsertionPoint |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ImageBaseBuilder.InsertionPoint |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ImageBaseBuilder.InsertionPoint[] |
values()
Returns an array that contains the values for this enum.
|
public static final ImageBaseBuilder.InsertionPoint DEFAULT
public static final ImageBaseBuilder.InsertionPoint USER_DEFINED
public static final int _DEFAULT
public static final int _USER_DEFINED
public static ImageBaseBuilder.InsertionPoint valueOf(int value)
public static ImageBaseBuilder.InsertionPoint valueOf(String name)
public static ImageBaseBuilder.InsertionPoint[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.