public static class IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HIGH
static image output resolution of 300 DPI (dots per inch)
|
static int |
_LOW
static image output resolution of 72 DPI (dots per inch)
|
static int |
_MEDIUM
static image output resolution of 150 DPI (dots per inch)
|
static int |
_USER_DEFINED
user specified image output resolution in DPI (dots per inch)
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
HIGH
static image output resolution of 300 DPI (dots per inch)
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
LOW
static image output resolution of 72 DPI (dots per inch)
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
MEDIUM
static image output resolution of 150 DPI (dots per inch)
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
USER_DEFINED
user specified image output resolution in DPI (dots per inch)
|
Modifier and Type | Method and Description |
---|---|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType HIGH
public static final IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType MEDIUM
public static final IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType LOW
public static final IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType USER_DEFINED
public static final int _HIGH
public static final int _MEDIUM
public static final int _LOW
public static final int _USER_DEFINED
public static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType valueOf(int value)
public static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType valueOf(String name)
public static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.