public interface DatumPlaneGridBuilder extends BoundedGridBuilder
DatumPlaneGrid
to a datum plane.
GridCollection.createDatumPlaneGridBuilder(nxopen.display.DatumPlaneGrid)
Property | Value |
---|---|
Associative | 1 |
GridOrientation | Custom |
LabelReference | Local |
MajorLineSpacing | 100 (millimeters part), 1 (inches part) |
MajorLineStyle | Solid |
MajorLineWeight | Normal |
MinorLineStyle | Dashed |
MinorLineWeight | Thin |
MinorLinesPerMajor | 1 |
Show | 1 |
ShowLabel | Always |
ShowMajorLines | 1 |
ShowOnTop | 0 |
SnapPointsPerMinor | 1 |
SnapToGrid | 0 |
Modifier and Type | Interface and Description |
---|---|
static class |
DatumPlaneGridBuilder.GridOrientationType
Specifies grid orientation option to be used for grid display.
|
BoundedGridBuilder.CornerPointsData, BoundedGridBuilder.LabelReferenceType, BoundedGridBuilder.ShowLabelType
GridBuilder.LineStyleType, GridBuilder.LineWeightType
Modifier and Type | Method and Description |
---|---|
DatumPlane[] |
getDatumPlanes()
Get the list of datum planes.
|
DatumPlaneGridBuilder.GridOrientationType |
gridOrientation()
Returns the grid orientation
License requirements: None. |
void |
setDatumPlanes(DatumPlane[] datumPlanes)
Set the list of datum planes.
|
void |
setGridOrientation(DatumPlaneGridBuilder.GridOrientationType gridOrientation)
License requirements: None. |
associative, getCornerPoints, labelReference, localOrigin, saveCurves, sectionCurveSettings, setAssociative, setCornerPoints, setLabelReference, setLocalOrigin, setShowLabel, showLabel
inheritSettings, lineColor, majorLineSpacing, majorLineStyle, majorLineWeight, minorLinesPerMajor, minorLineStyle, minorLineWeight, setLineColor, setMajorLineSpacing, setMajorLineStyle, setMajorLineWeight, setMinorLinesPerMajor, setMinorLineStyle, setMinorLineWeight, setShow, setShowMajorLines, setShowOnTop, setSnapPointsPerMinor, setSnapToGrid, show, showMajorLines, showOnTop, snapPointsPerMinor, snapToGrid
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
DatumPlane[] getDatumPlanes() throws NXException, RemoteException
NXException
RemoteException
void setDatumPlanes(DatumPlane[] datumPlanes) throws NXException, RemoteException
getDatumPlanes()
datumPlanes
- datum plane listNXException
RemoteException
DatumPlaneGridBuilder.GridOrientationType gridOrientation() throws NXException, RemoteException
NXException
RemoteException
void setGridOrientation(DatumPlaneGridBuilder.GridOrientationType gridOrientation) throws NXException, RemoteException
gridOrientation
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.