public interface CgfxMattexCollection extends TaggedObjectCollection
CgfxMattex
objects
BasePart
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
CgfxMattexBuilder |
createCgfxMattexBuilder(TaggedObject cgfxmattex)
Deprecated.
Deprecated in NX10.0.0. No alternative provided for this class.
|
TaggedObject |
find(String journalIdentifier)
Deprecated.
Deprecated in NX10.0.0. No alternative provided for this class.
|
_find_next, iterator
CgfxMattexBuilder createCgfxMattexBuilder(TaggedObject cgfxmattex) throws NXException, RemoteException
CgfxMattexBuilder
cgfxmattex
- If cgfxmattex is not null, then this object will be edited
NXException
RemoteException
TaggedObject find(String journalIdentifier) throws NXException, RemoteException
CgfxMattex
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Identifier to be foundNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.