CgfxMattexBuilder.TextureSpaceShader
instead.
public static class CgfxMattexBuilder.TextureSpace extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEFAULT_UV
Deprecated.
scale 1, 0 offset uv texture space
|
static int |
_EDITED
Deprecated.
the one edited using the material texture dialog
|
static CgfxMattexBuilder.TextureSpace |
DEFAULT_UV
Deprecated.
scale 1, 0 offset uv texture space
|
static CgfxMattexBuilder.TextureSpace |
EDITED
Deprecated.
the one edited using the material texture dialog
|
Modifier and Type | Method and Description |
---|---|
static CgfxMattexBuilder.TextureSpace |
valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static CgfxMattexBuilder.TextureSpace |
valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static CgfxMattexBuilder.TextureSpace[] |
values()
Deprecated.
Returns an array that contains the values for this enum.
|
public static final CgfxMattexBuilder.TextureSpace DEFAULT_UV
public static final CgfxMattexBuilder.TextureSpace EDITED
public static final int _DEFAULT_UV
public static final int _EDITED
public static CgfxMattexBuilder.TextureSpace valueOf(int value)
public static CgfxMattexBuilder.TextureSpace valueOf(String name)
public static CgfxMattexBuilder.TextureSpace[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.