public static class ThroatParentBuilder.TypeOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_RESTRIKE
Throat is built for a restrike operation.
|
static int |
_WIPE
Throat is built for a wipe operation.
|
static ThroatParentBuilder.TypeOption |
RESTRIKE
Throat is built for a restrike operation.
|
static ThroatParentBuilder.TypeOption |
WIPE
Throat is built for a wipe operation.
|
Modifier and Type | Method and Description |
---|---|
static ThroatParentBuilder.TypeOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThroatParentBuilder.TypeOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThroatParentBuilder.TypeOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final ThroatParentBuilder.TypeOption WIPE
public static final ThroatParentBuilder.TypeOption RESTRIKE
public static final int _WIPE
public static final int _RESTRIKE
public static ThroatParentBuilder.TypeOption valueOf(int value)
public static ThroatParentBuilder.TypeOption valueOf(String name)
public static ThroatParentBuilder.TypeOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.