public static class DrawBeadBuilder.ProjectionDirectionTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DRAW_DIRECTION
Project the centerline along the draw direction vector.
|
static int |
_NORMAL_TO_PLACEMENT_FACE
Project the centerline along the placement face normal.
|
static DrawBeadBuilder.ProjectionDirectionTypes |
DRAW_DIRECTION
Project the centerline along the draw direction vector.
|
static DrawBeadBuilder.ProjectionDirectionTypes |
NORMAL_TO_PLACEMENT_FACE
Project the centerline along the placement face normal.
|
Modifier and Type | Method and Description |
---|---|
static DrawBeadBuilder.ProjectionDirectionTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.ProjectionDirectionTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.ProjectionDirectionTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawBeadBuilder.ProjectionDirectionTypes DRAW_DIRECTION
public static final DrawBeadBuilder.ProjectionDirectionTypes NORMAL_TO_PLACEMENT_FACE
public static final int _DRAW_DIRECTION
public static final int _NORMAL_TO_PLACEMENT_FACE
public static DrawBeadBuilder.ProjectionDirectionTypes valueOf(int value)
public static DrawBeadBuilder.ProjectionDirectionTypes valueOf(String name)
public static DrawBeadBuilder.ProjectionDirectionTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.