public interface DieLocationsBuilder extends TaggedObject, IComponentBuilder
DieLocationsBuilder
. The Die
Locations is a helper to the main Die Design feature to gather the
location points for items such as hole center or clamping slot location.
Note that a non-point is selected, such as a plane or coordinate system,
the control point of the object will be used for the location.
DieCollection.createDieLocations(nxopen.features.Feature, boolean, boolean, boolean, boolean, boolean, boolean, boolean)
Modifier and Type | Method and Description |
---|---|
DieLocationBuilderList |
list()
Returns the list containing the die location objects
License requirements: None. |
printTestData, printTestData, tag, tagValue
validate
DieLocationBuilderList list() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.