public static class ClearanceBuilder.ClearanceGeometryTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SECTION
The input is closed profiles.
|
static int |
_SOLID
The input is solids.
|
static ClearanceBuilder.ClearanceGeometryTypes |
SECTION
The input is closed profiles.
|
static ClearanceBuilder.ClearanceGeometryTypes |
SOLID
The input is solids.
|
Modifier and Type | Method and Description |
---|---|
static ClearanceBuilder.ClearanceGeometryTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClearanceBuilder.ClearanceGeometryTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClearanceBuilder.ClearanceGeometryTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ClearanceBuilder.ClearanceGeometryTypes SOLID
public static final ClearanceBuilder.ClearanceGeometryTypes SECTION
public static final int _SOLID
public static final int _SECTION
public static ClearanceBuilder.ClearanceGeometryTypes valueOf(int value)
public static ClearanceBuilder.ClearanceGeometryTypes valueOf(String name)
public static ClearanceBuilder.ClearanceGeometryTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.