public interface CastReliefBuilder extends FeatureBuilder
CastReliefBuilder
builder
DieCollection.castRelief(nxopen.die.CastRelief)
Property | Value |
---|---|
AngleTolerance | 0.5 |
CreateSupportCasting | 0 |
DistanceTolerance | 0.0254 (millimeters part), 0.001 (inches part) |
ReliefDepth.Value | 5 (millimeters part), 0.2 (inches part) |
Thickness.Value | 35 (millimeters part), 1.4 (inches part) |
Modifier and Type | Method and Description |
---|---|
double |
angleTolerance()
Returns the angle tolerance
License requirements: None. |
DiePlaneBuilder |
baseOrientation()
Returns the base orientation of the die casting used for orienting the relief construction
License requirements: None. |
boolean |
createSupportCasting()
Returns the value (true or false) to decide if support casting should be created
License requirements: None. |
double |
distanceTolerance()
Returns the distance tolerance
License requirements: None. |
Expression |
reliefDepth()
Returns the depth value of the relief
License requirements: None. |
Section |
reliefProfile()
Returns the closed profiles used for determining the relief
License requirements: None. |
SelectNXObject |
reliefSheet()
Returns the sheet to offset to specify the relief surface
License requirements: None. |
void |
setAngleTolerance(double angleTolerance)
License requirements: ug_die_design ("Die Design") . |
void |
setCreateSupportCasting(boolean createSupportCasting)
License requirements: ug_die_design ("Die Design") . |
void |
setDistanceTolerance(double distanceTolerance)
License requirements: ug_die_design ("Die Design") . |
SelectNXObject |
sheetMetal()
Returns the sheet that specifies the sheet metal surface
License requirements: None. |
SelectNXObject |
target()
Returns the target solid the relief will be united with
License requirements: None. |
Expression |
thickness()
Returns the thickness value of the support casting surrounding the relief
License requirements: None. |
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectNXObject target() throws NXException, RemoteException
NXException
RemoteException
Section reliefProfile() throws NXException, RemoteException
NXException
RemoteException
SelectNXObject sheetMetal() throws NXException, RemoteException
NXException
RemoteException
SelectNXObject reliefSheet() throws NXException, RemoteException
NXException
RemoteException
DiePlaneBuilder baseOrientation() throws NXException, RemoteException
NXException
RemoteException
Expression reliefDepth() throws NXException, RemoteException
NXException
RemoteException
boolean createSupportCasting() throws NXException, RemoteException
NXException
RemoteException
void setCreateSupportCasting(boolean createSupportCasting) throws NXException, RemoteException
createSupportCasting
- NXException
RemoteException
Expression thickness() throws NXException, RemoteException
NXException
RemoteException
double distanceTolerance() throws NXException, RemoteException
NXException
RemoteException
void setDistanceTolerance(double distanceTolerance) throws NXException, RemoteException
distanceTolerance
- NXException
RemoteException
double angleTolerance() throws NXException, RemoteException
NXException
RemoteException
void setAngleTolerance(double angleTolerance) throws NXException, RemoteException
angleTolerance
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.