Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgCreator.OutputFileTypeOption |
DxfdwgCreator.OutputFileTypeOption.DWG
export data to DWG format
|
static DxfdwgCreator.OutputFileTypeOption |
DxfdwgCreator.OutputFileTypeOption.DXF
export data to DXF format
|
Modifier and Type | Method and Description |
---|---|
DxfdwgCreator.OutputFileTypeOption |
DxfdwgCreator.outputFileType()
Returns the output file type - this option determines the format of output file, It can either be dxf or dwg.
|
static DxfdwgCreator.OutputFileTypeOption |
DxfdwgCreator.OutputFileTypeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgCreator.OutputFileTypeOption |
DxfdwgCreator.OutputFileTypeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgCreator.OutputFileTypeOption[] |
DxfdwgCreator.OutputFileTypeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgCreator.setOutputFileType(DxfdwgCreator.OutputFileTypeOption outputFileType)
License requirements: None. |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.