Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
BasePropertyTable |
PhysicalMaterial.getPropTable()
Returns the property table that contains the properties for this material.
|
Modifier and Type | Method and Description |
---|---|
void |
BasePropertyTable.copyProperties(BasePropertyTable sourceTable)
Copies the values from the input table into this table, the table descriptor neutral names must match
License requirements: None. |
void |
BasePropertyTable.copyProperty(String propertyName,
BasePropertyTable sourcePropertyTable)
Copy the value of one property from the source table into this table
License requirements: None. |
Modifier and Type | Interface and Description |
---|---|
interface |
PropertyTable
Represents a property table
This is a sub object . |
Modifier and Type | Method and Description |
---|---|
BasePropertyTable |
SimLoadRecipeSource.getPropertyTable()
Get the
BasePropertyTable of a SimLoadRecipeSource . |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.