Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
nxopen.cam.fbm |
Provides classes and interfaces relating to Features Based Modeling.
|
Class and Description |
---|
Feature
Interface for CAM Feature objects
This is an abstract class, and cannot be instantiated. |
FeatureGeometry
Represents a feature geometry builder
This is an abstract class and cannot be instantiated. |
MachiningFeatureGeometry
Represents a feature geometry builder
An instance of this class can be obtained from CAM.HoleBossGeom#getCenterHoleGeometry or CAM.HoleBossGeom#getChamferHoleGeometry Created in NX9.0.0 |
Class and Description |
---|
Feature
Interface for CAM Feature objects
This is an abstract class, and cannot be instantiated. |
FeatureGeometry
Represents a feature geometry builder
This is an abstract class and cannot be instantiated. |
FeatureGeometry.SequenceDirectionType
the direction types .
|
FeatureGeometry.SequencePatternType
the pattern types .
|
FeatureGeometry.SortOrder
the optimization types .
|
FeatureSet
Interface for feature set
To create a new instance of this class, use FeatureGeometry.createFeatureSet() Created in NX9.0.0 |
ThreadFeatureGeometry.Form
Thread form standards .
|
ThreadFeatureGeometry.Rotation
the rotation types .
|
ThreadFeatureGeometry.ThreadDataSource
thread data source types .
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.