public static class WedmOperationBuilder.InPathUdeSetTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END
in path ude set at end
|
static int |
_START
in path ude set at start
|
static WedmOperationBuilder.InPathUdeSetTypes |
END
in path ude set at end
|
static WedmOperationBuilder.InPathUdeSetTypes |
START
in path ude set at start
|
Modifier and Type | Method and Description |
---|---|
static WedmOperationBuilder.InPathUdeSetTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WedmOperationBuilder.InPathUdeSetTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WedmOperationBuilder.InPathUdeSetTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final WedmOperationBuilder.InPathUdeSetTypes START
public static final WedmOperationBuilder.InPathUdeSetTypes END
public static final int _START
public static final int _END
public static WedmOperationBuilder.InPathUdeSetTypes valueOf(int value)
public static WedmOperationBuilder.InPathUdeSetTypes valueOf(String name)
public static WedmOperationBuilder.InPathUdeSetTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.