public static class TurnFeatureGeomBuilder.SurfaceSensitivityModes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISTANCE
Surface sensitivity is active.
|
static int |
_NONE
Surface sensitivity is inactive.
|
static TurnFeatureGeomBuilder.SurfaceSensitivityModes |
DISTANCE
Surface sensitivity is active.
|
static TurnFeatureGeomBuilder.SurfaceSensitivityModes |
NONE
Surface sensitivity is inactive.
|
Modifier and Type | Method and Description |
---|---|
static TurnFeatureGeomBuilder.SurfaceSensitivityModes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnFeatureGeomBuilder.SurfaceSensitivityModes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnFeatureGeomBuilder.SurfaceSensitivityModes[] |
values()
Returns an array that contains the values for this enum.
|
public static final TurnFeatureGeomBuilder.SurfaceSensitivityModes NONE
public static final TurnFeatureGeomBuilder.SurfaceSensitivityModes DISTANCE
public static final int _NONE
public static final int _DISTANCE
public static TurnFeatureGeomBuilder.SurfaceSensitivityModes valueOf(int value)
public static TurnFeatureGeomBuilder.SurfaceSensitivityModes valueOf(String name)
public static TurnFeatureGeomBuilder.SurfaceSensitivityModes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.