public static class TurnAvoidanceStartBuilder.StartPointMotionTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AXIAL_THEN_RADIAL
Motion type: Axial then axial to point.
|
static int |
_CLEAR_AXIAL_THEN_DIRECT
Motion type: Axial to clearance plane then direct to point.
|
static int |
_CLEAR_RADIAL_THEN_DIRECT
Motion type: Radial to clearance plane then direct to point.
|
static int |
_DIRECT
Motion type: Direct to point.
|
static int |
_NONE
Point is inactive.
|
static int |
_RADIAL_THEN_AXIAL
Motion type: Radial then axial to point.
|
static TurnAvoidanceStartBuilder.StartPointMotionTypes |
AXIAL_THEN_RADIAL
Motion type: Axial then axial to point.
|
static TurnAvoidanceStartBuilder.StartPointMotionTypes |
CLEAR_AXIAL_THEN_DIRECT
Motion type: Axial to clearance plane then direct to point.
|
static TurnAvoidanceStartBuilder.StartPointMotionTypes |
CLEAR_RADIAL_THEN_DIRECT
Motion type: Radial to clearance plane then direct to point.
|
static TurnAvoidanceStartBuilder.StartPointMotionTypes |
DIRECT
Motion type: Direct to point.
|
static TurnAvoidanceStartBuilder.StartPointMotionTypes |
NONE
Point is inactive.
|
static TurnAvoidanceStartBuilder.StartPointMotionTypes |
RADIAL_THEN_AXIAL
Motion type: Radial then axial to point.
|
Modifier and Type | Method and Description |
---|---|
static TurnAvoidanceStartBuilder.StartPointMotionTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceStartBuilder.StartPointMotionTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceStartBuilder.StartPointMotionTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final TurnAvoidanceStartBuilder.StartPointMotionTypes NONE
public static final TurnAvoidanceStartBuilder.StartPointMotionTypes DIRECT
public static final TurnAvoidanceStartBuilder.StartPointMotionTypes RADIAL_THEN_AXIAL
public static final TurnAvoidanceStartBuilder.StartPointMotionTypes AXIAL_THEN_RADIAL
public static final TurnAvoidanceStartBuilder.StartPointMotionTypes CLEAR_RADIAL_THEN_DIRECT
public static final TurnAvoidanceStartBuilder.StartPointMotionTypes CLEAR_AXIAL_THEN_DIRECT
public static final int _NONE
public static final int _DIRECT
public static final int _RADIAL_THEN_AXIAL
public static final int _AXIAL_THEN_RADIAL
public static final int _CLEAR_RADIAL_THEN_DIRECT
public static final int _CLEAR_AXIAL_THEN_DIRECT
public static TurnAvoidanceStartBuilder.StartPointMotionTypes valueOf(int value)
public static TurnAvoidanceStartBuilder.StartPointMotionTypes valueOf(String name)
public static TurnAvoidanceStartBuilder.StartPointMotionTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.