public interface SpringPasses extends TaggedObject
Modifier and Type | Interface and Description |
---|---|
static class |
SpringPasses.Types
the alternate spring passes options .
|
Modifier and Type | Method and Description |
---|---|
int |
number()
Returns the number of spring passes
License requirements: None. |
void |
setNumber(int springPasses)
License requirements: cam_base ("CAM BASE") . |
void |
setType(SpringPasses.Types alternateSpringPassesMode)
License requirements: cam_base ("CAM BASE") . |
SpringPasses.Types |
type()
Returns the type of spring passes
License requirements: None. |
printTestData, printTestData, tag, tagValue
int number() throws NXException, RemoteException
NXException
RemoteException
void setNumber(int springPasses) throws NXException, RemoteException
springPasses
- the number of spring passesNXException
RemoteException
SpringPasses.Types type() throws NXException, RemoteException
NXException
RemoteException
void setType(SpringPasses.Types alternateSpringPassesMode) throws NXException, RemoteException
alternateSpringPassesMode
- the type of spring passesNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.