public static class ProbeInspectSurfacePointMoveBuilder.ToolAxis extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
Tool Axis aligned with closest machine axis
|
static int |
_NONE
Use the Previous Tool Axis
|
static int |
_NORMAL
Inferred using surface normal
|
static ProbeInspectSurfacePointMoveBuilder.ToolAxis |
AUTOMATIC
Tool Axis aligned with closest machine axis
|
static ProbeInspectSurfacePointMoveBuilder.ToolAxis |
NONE
Use the Previous Tool Axis
|
static ProbeInspectSurfacePointMoveBuilder.ToolAxis |
NORMAL
Inferred using surface normal
|
Modifier and Type | Method and Description |
---|---|
static ProbeInspectSurfacePointMoveBuilder.ToolAxis |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProbeInspectSurfacePointMoveBuilder.ToolAxis |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProbeInspectSurfacePointMoveBuilder.ToolAxis[] |
values()
Returns an array that contains the values for this enum.
|
public static final ProbeInspectSurfacePointMoveBuilder.ToolAxis NONE
public static final ProbeInspectSurfacePointMoveBuilder.ToolAxis NORMAL
public static final ProbeInspectSurfacePointMoveBuilder.ToolAxis AUTOMATIC
public static final int _NONE
public static final int _NORMAL
public static final int _AUTOMATIC
public static ProbeInspectSurfacePointMoveBuilder.ToolAxis valueOf(int value)
public static ProbeInspectSurfacePointMoveBuilder.ToolAxis valueOf(String name)
public static ProbeInspectSurfacePointMoveBuilder.ToolAxis[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.