public static class OperationTransformBuilder.Angle extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SPECIFY
specify a angle
|
static int |
_TWO_POINT
use two point to sepcify a angle
|
static OperationTransformBuilder.Angle |
SPECIFY
specify a angle
|
static OperationTransformBuilder.Angle |
TWO_POINT
use two point to sepcify a angle
|
Modifier and Type | Method and Description |
---|---|
static OperationTransformBuilder.Angle |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OperationTransformBuilder.Angle |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OperationTransformBuilder.Angle[] |
values()
Returns an array that contains the values for this enum.
|
public static final OperationTransformBuilder.Angle SPECIFY
public static final OperationTransformBuilder.Angle TWO_POINT
public static final int _SPECIFY
public static final int _TWO_POINT
public static OperationTransformBuilder.Angle valueOf(int value)
public static OperationTransformBuilder.Angle valueOf(String name)
public static OperationTransformBuilder.Angle[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.