public static class InspectionSurfaceFeatureBuilder.PointDataDefinitionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INDIVIDUAL_POINTS
Individual points are defined
|
static int |
_NONE
No point data is defined
|
static int |
_POINT_SET
A set of points are defined using parameters
|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
INDIVIDUAL_POINTS
Individual points are defined
|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
NONE
No point data is defined
|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
POINT_SET
A set of points are defined using parameters
|
Modifier and Type | Method and Description |
---|---|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionSurfaceFeatureBuilder.PointDataDefinitionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionSurfaceFeatureBuilder.PointDataDefinitionType NONE
public static final InspectionSurfaceFeatureBuilder.PointDataDefinitionType POINT_SET
public static final InspectionSurfaceFeatureBuilder.PointDataDefinitionType INDIVIDUAL_POINTS
public static final int _NONE
public static final int _POINT_SET
public static final int _INDIVIDUAL_POINTS
public static InspectionSurfaceFeatureBuilder.PointDataDefinitionType valueOf(int value)
public static InspectionSurfaceFeatureBuilder.PointDataDefinitionType valueOf(String name)
public static InspectionSurfaceFeatureBuilder.PointDataDefinitionType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.