public static class InspectionMoveBuilder.SensorStrategyTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CREATE_AS_NEEDED
Create as needed
|
static int |
_USE_EXISTING
Use existing only
|
static InspectionMoveBuilder.SensorStrategyTypes |
CREATE_AS_NEEDED
Create as needed
|
static InspectionMoveBuilder.SensorStrategyTypes |
USE_EXISTING
Use existing only
|
Modifier and Type | Method and Description |
---|---|
static InspectionMoveBuilder.SensorStrategyTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionMoveBuilder.SensorStrategyTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionMoveBuilder.SensorStrategyTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionMoveBuilder.SensorStrategyTypes CREATE_AS_NEEDED
public static final InspectionMoveBuilder.SensorStrategyTypes USE_EXISTING
public static final int _CREATE_AS_NEEDED
public static final int _USE_EXISTING
public static InspectionMoveBuilder.SensorStrategyTypes valueOf(int value)
public static InspectionMoveBuilder.SensorStrategyTypes valueOf(String name)
public static InspectionMoveBuilder.SensorStrategyTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.