public static class InspectionMethodBuilder.LimitsOfSizeTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AVERAGE
Average
|
static int |
_FUNCTIONAL
Functional
|
static int |
_TWO_POINT
Two Point
|
static InspectionMethodBuilder.LimitsOfSizeTypes |
AVERAGE
Average
|
static InspectionMethodBuilder.LimitsOfSizeTypes |
FUNCTIONAL
Functional
|
static InspectionMethodBuilder.LimitsOfSizeTypes |
TWO_POINT
Two Point
|
Modifier and Type | Method and Description |
---|---|
static InspectionMethodBuilder.LimitsOfSizeTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionMethodBuilder.LimitsOfSizeTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionMethodBuilder.LimitsOfSizeTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionMethodBuilder.LimitsOfSizeTypes AVERAGE
public static final InspectionMethodBuilder.LimitsOfSizeTypes FUNCTIONAL
public static final InspectionMethodBuilder.LimitsOfSizeTypes TWO_POINT
public static final int _AVERAGE
public static final int _FUNCTIONAL
public static final int _TWO_POINT
public static InspectionMethodBuilder.LimitsOfSizeTypes valueOf(int value)
public static InspectionMethodBuilder.LimitsOfSizeTypes valueOf(String name)
public static InspectionMethodBuilder.LimitsOfSizeTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.