public static class InspectionConstructedFeatureBuilder.CurrentStateType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ACTUAL
Feature is an actual measured feature
|
static int |
_NOMINAL
Feature is in its nominal (design) state
|
static InspectionConstructedFeatureBuilder.CurrentStateType |
ACTUAL
Feature is an actual measured feature
|
static InspectionConstructedFeatureBuilder.CurrentStateType |
NOMINAL
Feature is in its nominal (design) state
|
Modifier and Type | Method and Description |
---|---|
static InspectionConstructedFeatureBuilder.CurrentStateType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionConstructedFeatureBuilder.CurrentStateType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionConstructedFeatureBuilder.CurrentStateType[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionConstructedFeatureBuilder.CurrentStateType NOMINAL
public static final InspectionConstructedFeatureBuilder.CurrentStateType ACTUAL
public static final int _NOMINAL
public static final int _ACTUAL
public static InspectionConstructedFeatureBuilder.CurrentStateType valueOf(int value)
public static InspectionConstructedFeatureBuilder.CurrentStateType valueOf(String name)
public static InspectionConstructedFeatureBuilder.CurrentStateType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.