public static class GougeCheckResults.Constants extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAX_GOUGES
The maximum number of gouges
|
static GougeCheckResults.Constants |
MAX_GOUGES
The maximum number of gouges
|
Modifier and Type | Method and Description |
---|---|
static GougeCheckResults.Constants |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GougeCheckResults.Constants |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GougeCheckResults.Constants[] |
values()
Returns an array that contains the values for this enum.
|
public static final GougeCheckResults.Constants MAX_GOUGES
public static final int _MAX_GOUGES
public static GougeCheckResults.Constants valueOf(int value)
public static GougeCheckResults.Constants valueOf(String name)
public static GougeCheckResults.Constants[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.