public static class FeatureProcessBuilder.FeatureProcessType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_RULE_BASED
Rule based operation creation
|
static int |
_TEMPLATE_BASED
Template based operation creation
|
static FeatureProcessBuilder.FeatureProcessType |
RULE_BASED
Rule based operation creation
|
static FeatureProcessBuilder.FeatureProcessType |
TEMPLATE_BASED
Template based operation creation
|
Modifier and Type | Method and Description |
---|---|
static FeatureProcessBuilder.FeatureProcessType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FeatureProcessBuilder.FeatureProcessType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FeatureProcessBuilder.FeatureProcessType[] |
values()
Returns an array that contains the values for this enum.
|
public static final FeatureProcessBuilder.FeatureProcessType RULE_BASED
public static final FeatureProcessBuilder.FeatureProcessType TEMPLATE_BASED
public static final int _RULE_BASED
public static final int _TEMPLATE_BASED
public static FeatureProcessBuilder.FeatureProcessType valueOf(int value)
public static FeatureProcessBuilder.FeatureProcessType valueOf(String name)
public static FeatureProcessBuilder.FeatureProcessType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.