public static class CAMObject.Status extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_APPROVED
Object path has been approved as is
|
static int |
_COMPLETE
Object path has been output
|
static int |
_REGEN
Object path must be regenerated
|
static int |
_REPOST
Object path must be post-processed
|
static CAMObject.Status |
APPROVED
Object path has been approved as is
|
static CAMObject.Status |
COMPLETE
Object path has been output
|
static CAMObject.Status |
REGEN
Object path must be regenerated
|
static CAMObject.Status |
REPOST
Object path must be post-processed
|
Modifier and Type | Method and Description |
---|---|
static CAMObject.Status |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAMObject.Status |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAMObject.Status[] |
values()
Returns an array that contains the values for this enum.
|
public static final CAMObject.Status COMPLETE
public static final CAMObject.Status REPOST
public static final CAMObject.Status REGEN
public static final CAMObject.Status APPROVED
public static final int _COMPLETE
public static final int _REPOST
public static final int _REGEN
public static final int _APPROVED
public static CAMObject.Status valueOf(int value)
public static CAMObject.Status valueOf(String name)
public static CAMObject.Status[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.