public static class CAMFeature.ProcessStatus extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COMPLETE
The feature's operation toolpaths are complete
|
static int |
_EMPTY
Feature has no operations
|
static int |
_INCOMPLETE
One or more of the feature's operation toolpaths are not completed
|
static int |
_REGENERATE
One or more of the feature's operation toolpaths need to regenerate
|
static CAMFeature.ProcessStatus |
COMPLETE
The feature's operation toolpaths are complete
|
static CAMFeature.ProcessStatus |
EMPTY
Feature has no operations
|
static CAMFeature.ProcessStatus |
INCOMPLETE
One or more of the feature's operation toolpaths are not completed
|
static CAMFeature.ProcessStatus |
REGENERATE
One or more of the feature's operation toolpaths need to regenerate
|
Modifier and Type | Method and Description |
---|---|
static CAMFeature.ProcessStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAMFeature.ProcessStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAMFeature.ProcessStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final CAMFeature.ProcessStatus EMPTY
public static final CAMFeature.ProcessStatus REGENERATE
public static final CAMFeature.ProcessStatus INCOMPLETE
public static final CAMFeature.ProcessStatus COMPLETE
public static final int _EMPTY
public static final int _REGENERATE
public static final int _INCOMPLETE
public static final int _COMPLETE
public static CAMFeature.ProcessStatus valueOf(int value)
public static CAMFeature.ProcessStatus valueOf(String name)
public static CAMFeature.ProcessStatus[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.