public class PhaseRangeOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NEGATIVE_HALF_PI_TO_ONE_HALF_PI
Displays phase between -90 and 270
|
static int |
_NEGATIVE_ONE_HALF_PI_TO_HALF_PI
Displays phase between -270 and 90
|
static int |
_NEGATIVE_PI_TO_PI
Displays phase between -180 and 180
|
static int |
_NEGATIVE_TWO_PI_TO_ZERO
Displays phase between -360 and 0
|
static int |
_ZERO_TO_TWO_PI
Displays phase between 0 and 360
|
static PhaseRangeOption |
NEGATIVE_HALF_PI_TO_ONE_HALF_PI
Displays phase between -90 and 270
|
static PhaseRangeOption |
NEGATIVE_ONE_HALF_PI_TO_HALF_PI
Displays phase between -270 and 90
|
static PhaseRangeOption |
NEGATIVE_PI_TO_PI
Displays phase between -180 and 180
|
static PhaseRangeOption |
NEGATIVE_TWO_PI_TO_ZERO
Displays phase between -360 and 0
|
static PhaseRangeOption |
ZERO_TO_TWO_PI
Displays phase between 0 and 360
|
Modifier and Type | Method and Description |
---|---|
static PhaseRangeOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PhaseRangeOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PhaseRangeOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final PhaseRangeOption NEGATIVE_TWO_PI_TO_ZERO
public static final PhaseRangeOption ZERO_TO_TWO_PI
public static final PhaseRangeOption NEGATIVE_PI_TO_PI
public static final PhaseRangeOption NEGATIVE_ONE_HALF_PI_TO_HALF_PI
public static final PhaseRangeOption NEGATIVE_HALF_PI_TO_ONE_HALF_PI
public static final int _NEGATIVE_TWO_PI_TO_ZERO
public static final int _ZERO_TO_TWO_PI
public static final int _NEGATIVE_PI_TO_PI
public static final int _NEGATIVE_ONE_HALF_PI_TO_HALF_PI
public static final int _NEGATIVE_HALF_PI_TO_ONE_HALF_PI
public static PhaseRangeOption valueOf(int value)
public static PhaseRangeOption valueOf(String name)
public static PhaseRangeOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.