public class ContouringRange extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BORDER_GRID
Option to show contour range on the border of the grid
|
static int |
_FULL_GRID
Option to show contour range on the face of the grid
|
static ContouringRange |
BORDER_GRID
Option to show contour range on the border of the grid
|
static ContouringRange |
FULL_GRID
Option to show contour range on the face of the grid
|
Modifier and Type | Method and Description |
---|---|
static ContouringRange |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ContouringRange |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ContouringRange[] |
values()
Returns an array that contains the values for this enum.
|
public static final ContouringRange BORDER_GRID
public static final ContouringRange FULL_GRID
public static final int _BORDER_GRID
public static final int _FULL_GRID
public static ContouringRange valueOf(int value)
public static ContouringRange valueOf(String name)
public static ContouringRange[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.