public static class VelocityImpactDirection.NodalComponentType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DOF1 |
static int |
_DOF2 |
static int |
_DOF3 |
static VelocityImpactDirection.NodalComponentType |
DOF1 |
static VelocityImpactDirection.NodalComponentType |
DOF2 |
static VelocityImpactDirection.NodalComponentType |
DOF3 |
Modifier and Type | Method and Description |
---|---|
static VelocityImpactDirection.NodalComponentType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static VelocityImpactDirection.NodalComponentType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static VelocityImpactDirection.NodalComponentType[] |
values()
Returns an array that contains the values for this enum.
|
public static final VelocityImpactDirection.NodalComponentType DOF1
public static final VelocityImpactDirection.NodalComponentType DOF2
public static final VelocityImpactDirection.NodalComponentType DOF3
public static final int _DOF1
public static final int _DOF2
public static final int _DOF3
public static VelocityImpactDirection.NodalComponentType valueOf(int value)
public static VelocityImpactDirection.NodalComponentType valueOf(String name)
public static VelocityImpactDirection.NodalComponentType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.