public class ResponseDomainDefinitionMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_KEY_IN |
static int |
_NATURAL_FREQUENCY |
static int |
_START_END_POINT |
static ResponseDomainDefinitionMethod |
KEY_IN |
static ResponseDomainDefinitionMethod |
NATURAL_FREQUENCY |
static ResponseDomainDefinitionMethod |
START_END_POINT |
Modifier and Type | Method and Description |
---|---|
static ResponseDomainDefinitionMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResponseDomainDefinitionMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResponseDomainDefinitionMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final ResponseDomainDefinitionMethod START_END_POINT
public static final ResponseDomainDefinitionMethod KEY_IN
public static final ResponseDomainDefinitionMethod NATURAL_FREQUENCY
public static final int _START_END_POINT
public static final int _KEY_IN
public static final int _NATURAL_FREQUENCY
public static ResponseDomainDefinitionMethod valueOf(int value)
public static ResponseDomainDefinitionMethod valueOf(String name)
public static ResponseDomainDefinitionMethod[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.