public static class InitialConditions.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_QUASI_STATIC |
static int |
_USER_DEFINED |
static int |
_ZERO |
static InitialConditions.Type |
QUASI_STATIC |
static InitialConditions.Type |
USER_DEFINED |
static InitialConditions.Type |
ZERO |
Modifier and Type | Method and Description |
---|---|
static InitialConditions.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InitialConditions.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InitialConditions.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final InitialConditions.Type QUASI_STATIC
public static final InitialConditions.Type ZERO
public static final InitialConditions.Type USER_DEFINED
public static final int _QUASI_STATIC
public static final int _ZERO
public static final int _USER_DEFINED
public static InitialConditions.Type valueOf(int value)
public static InitialConditions.Type valueOf(String name)
public static InitialConditions.Type[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.