public static class ExcitationBuilder.ExcitationLocationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISTRIBUTED_LOAD |
static int |
_ENFORCED_MOTION |
static int |
_NODAL_FORCE |
static int |
_STATIC_LOAD |
static ExcitationBuilder.ExcitationLocationType |
DISTRIBUTED_LOAD |
static ExcitationBuilder.ExcitationLocationType |
ENFORCED_MOTION |
static ExcitationBuilder.ExcitationLocationType |
NODAL_FORCE |
static ExcitationBuilder.ExcitationLocationType |
STATIC_LOAD |
Modifier and Type | Method and Description |
---|---|
static ExcitationBuilder.ExcitationLocationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExcitationBuilder.ExcitationLocationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExcitationBuilder.ExcitationLocationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ExcitationBuilder.ExcitationLocationType STATIC_LOAD
public static final ExcitationBuilder.ExcitationLocationType DISTRIBUTED_LOAD
public static final ExcitationBuilder.ExcitationLocationType NODAL_FORCE
public static final ExcitationBuilder.ExcitationLocationType ENFORCED_MOTION
public static final int _STATIC_LOAD
public static final int _DISTRIBUTED_LOAD
public static final int _NODAL_FORCE
public static final int _ENFORCED_MOTION
public static ExcitationBuilder.ExcitationLocationType valueOf(int value)
public static ExcitationBuilder.ExcitationLocationType valueOf(String name)
public static ExcitationBuilder.ExcitationLocationType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.