public static class TBSTopologySensitivityOptimizationParameters.MaterialInterpolation extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_RAMP
Rational approximation of material properties
|
static int |
_SIMP
Solid Isotropic material with penalization
|
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
RAMP
Rational approximation of material properties
|
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
SIMP
Solid Isotropic material with penalization
|
Modifier and Type | Method and Description |
---|---|
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSTopologySensitivityOptimizationParameters.MaterialInterpolation SIMP
public static final TBSTopologySensitivityOptimizationParameters.MaterialInterpolation RAMP
public static final int _SIMP
public static final int _RAMP
public static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation valueOf(int value)
public static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation valueOf(String name)
public static TBSTopologySensitivityOptimizationParameters.MaterialInterpolation[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.