public static class TBSTopologyLinkCondition.SymmetryOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CYCLIC_SYMMETRY
Cyclic symmetry definition
|
static int |
_PLANE_SYMMETRY
Plane symmetry referring to the plane which lies
perpendicular to the given axis of the coordinate system
|
static TBSTopologyLinkCondition.SymmetryOption |
CYCLIC_SYMMETRY
Cyclic symmetry definition
|
static TBSTopologyLinkCondition.SymmetryOption |
PLANE_SYMMETRY
Plane symmetry referring to the plane which lies
perpendicular to the given axis of the coordinate system
|
Modifier and Type | Method and Description |
---|---|
static TBSTopologyLinkCondition.SymmetryOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologyLinkCondition.SymmetryOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologyLinkCondition.SymmetryOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSTopologyLinkCondition.SymmetryOption PLANE_SYMMETRY
public static final TBSTopologyLinkCondition.SymmetryOption CYCLIC_SYMMETRY
public static final int _PLANE_SYMMETRY
public static final int _CYCLIC_SYMMETRY
public static TBSTopologyLinkCondition.SymmetryOption valueOf(int value)
public static TBSTopologyLinkCondition.SymmetryOption valueOf(String name)
public static TBSTopologyLinkCondition.SymmetryOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.