public static class TBSTopologyControllerOptimizationParameters.AutoFrozen extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BOTH
All loaded elements, elements with load nodes with boundary conditions are excluded from the optimization
|
static int |
_LOAD
All loaded elements and nodes are excluded from the optimization
|
static int |
_OFF
Loaded elements are optimizable
|
static int |
_SPC
Elements with boundary conditions are excluded from the optimization
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
BOTH
All loaded elements, elements with load nodes with boundary conditions are excluded from the optimization
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
LOAD
All loaded elements and nodes are excluded from the optimization
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
OFF
Loaded elements are optimizable
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
SPC
Elements with boundary conditions are excluded from the optimization
|
Modifier and Type | Method and Description |
---|---|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologyControllerOptimizationParameters.AutoFrozen[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSTopologyControllerOptimizationParameters.AutoFrozen LOAD
public static final TBSTopologyControllerOptimizationParameters.AutoFrozen OFF
public static final TBSTopologyControllerOptimizationParameters.AutoFrozen SPC
public static final TBSTopologyControllerOptimizationParameters.AutoFrozen BOTH
public static final int _LOAD
public static final int _OFF
public static final int _SPC
public static final int _BOTH
public static TBSTopologyControllerOptimizationParameters.AutoFrozen valueOf(int value)
public static TBSTopologyControllerOptimizationParameters.AutoFrozen valueOf(String name)
public static TBSTopologyControllerOptimizationParameters.AutoFrozen[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.