public static class TBSSmoothBuilder.OriginalSurfaceSmoothingOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FULL
Allows any modifications to the original surface
|
static int |
_OFF
No changes to the original surface
|
static int |
_SHRINK
Allows the nodes on original surface to be moved towards the inside only
|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
FULL
Allows any modifications to the original surface
|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
OFF
No changes to the original surface
|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
SHRINK
Allows the nodes on original surface to be moved towards the inside only
|
Modifier and Type | Method and Description |
---|---|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSSmoothBuilder.OriginalSurfaceSmoothingOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSSmoothBuilder.OriginalSurfaceSmoothingOption OFF
public static final TBSSmoothBuilder.OriginalSurfaceSmoothingOption SHRINK
public static final TBSSmoothBuilder.OriginalSurfaceSmoothingOption FULL
public static final int _OFF
public static final int _SHRINK
public static final int _FULL
public static TBSSmoothBuilder.OriginalSurfaceSmoothingOption valueOf(int value)
public static TBSSmoothBuilder.OriginalSurfaceSmoothingOption valueOf(String name)
public static TBSSmoothBuilder.OriginalSurfaceSmoothingOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.