public static class TBSOptimizationSolutionBuilder.StrategyType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONTROLLER
uses controller strategy to run optimization
|
static int |
_SENSITIVITY
Uses sensitivity strategy to run optimization
|
static TBSOptimizationSolutionBuilder.StrategyType |
CONTROLLER
uses controller strategy to run optimization
|
static TBSOptimizationSolutionBuilder.StrategyType |
SENSITIVITY
Uses sensitivity strategy to run optimization
|
Modifier and Type | Method and Description |
---|---|
static TBSOptimizationSolutionBuilder.StrategyType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSOptimizationSolutionBuilder.StrategyType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSOptimizationSolutionBuilder.StrategyType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSOptimizationSolutionBuilder.StrategyType SENSITIVITY
public static final TBSOptimizationSolutionBuilder.StrategyType CONTROLLER
public static final int _SENSITIVITY
public static final int _CONTROLLER
public static TBSOptimizationSolutionBuilder.StrategyType valueOf(int value)
public static TBSOptimizationSolutionBuilder.StrategyType valueOf(String name)
public static TBSOptimizationSolutionBuilder.StrategyType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.