public static class TBSLoadCaseManager.SelectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAXIMUM
Maximum value of the selected load cases
|
static int |
_MINIMUM
Minimum value of the selected load cases
|
static int |
_SUM
Sum of the selected load cases
|
static TBSLoadCaseManager.SelectionType |
MAXIMUM
Maximum value of the selected load cases
|
static TBSLoadCaseManager.SelectionType |
MINIMUM
Minimum value of the selected load cases
|
static TBSLoadCaseManager.SelectionType |
SUM
Sum of the selected load cases
|
Modifier and Type | Method and Description |
---|---|
static TBSLoadCaseManager.SelectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSLoadCaseManager.SelectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSLoadCaseManager.SelectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSLoadCaseManager.SelectionType MAXIMUM
public static final TBSLoadCaseManager.SelectionType MINIMUM
public static final TBSLoadCaseManager.SelectionType SUM
public static final int _MAXIMUM
public static final int _MINIMUM
public static final int _SUM
public static TBSLoadCaseManager.SelectionType valueOf(int value)
public static TBSLoadCaseManager.SelectionType valueOf(String name)
public static TBSLoadCaseManager.SelectionType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.