public static class SimLoadRecipeTypes.LoadConditionHandling extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PER_DATA_SOURCE
Treat each source as a load condition
|
static int |
_SINGLE
Treat all sources as a single load condition
|
static SimLoadRecipeTypes.LoadConditionHandling |
PER_DATA_SOURCE
Treat each source as a load condition
|
static SimLoadRecipeTypes.LoadConditionHandling |
SINGLE
Treat all sources as a single load condition
|
Modifier and Type | Method and Description |
---|---|
static SimLoadRecipeTypes.LoadConditionHandling |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimLoadRecipeTypes.LoadConditionHandling |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimLoadRecipeTypes.LoadConditionHandling[] |
values()
Returns an array that contains the values for this enum.
|
public static final SimLoadRecipeTypes.LoadConditionHandling SINGLE
public static final SimLoadRecipeTypes.LoadConditionHandling PER_DATA_SOURCE
public static final int _SINGLE
public static final int _PER_DATA_SOURCE
public static SimLoadRecipeTypes.LoadConditionHandling valueOf(int value)
public static SimLoadRecipeTypes.LoadConditionHandling valueOf(String name)
public static SimLoadRecipeTypes.LoadConditionHandling[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.