public static class SimBcPlotContoursBuilder.ResolveOverlapType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADD |
static int |
_AVERAGE |
static int |
_MAXIMUM |
static int |
_MINIMUM |
static int |
_SPECIFY |
static SimBcPlotContoursBuilder.ResolveOverlapType |
ADD |
static SimBcPlotContoursBuilder.ResolveOverlapType |
AVERAGE |
static SimBcPlotContoursBuilder.ResolveOverlapType |
MAXIMUM |
static SimBcPlotContoursBuilder.ResolveOverlapType |
MINIMUM |
static SimBcPlotContoursBuilder.ResolveOverlapType |
SPECIFY |
Modifier and Type | Method and Description |
---|---|
static SimBcPlotContoursBuilder.ResolveOverlapType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimBcPlotContoursBuilder.ResolveOverlapType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimBcPlotContoursBuilder.ResolveOverlapType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SimBcPlotContoursBuilder.ResolveOverlapType ADD
public static final SimBcPlotContoursBuilder.ResolveOverlapType AVERAGE
public static final SimBcPlotContoursBuilder.ResolveOverlapType MAXIMUM
public static final SimBcPlotContoursBuilder.ResolveOverlapType MINIMUM
public static final SimBcPlotContoursBuilder.ResolveOverlapType SPECIFY
public static final int _ADD
public static final int _AVERAGE
public static final int _MAXIMUM
public static final int _MINIMUM
public static final int _SPECIFY
public static SimBcPlotContoursBuilder.ResolveOverlapType valueOf(int value)
public static SimBcPlotContoursBuilder.ResolveOverlapType valueOf(String name)
public static SimBcPlotContoursBuilder.ResolveOverlapType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.