public static class ResultProbeBuilder.GeometryValue extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ARITHMETIC_MEAN |
static int |
_INTEGRAL |
static int |
_MAXIMUM |
static int |
_MINIMUM |
static int |
_NONE |
static int |
_SUM |
static int |
_WEIGHTED_AVERAGE |
static ResultProbeBuilder.GeometryValue |
ARITHMETIC_MEAN |
static ResultProbeBuilder.GeometryValue |
INTEGRAL |
static ResultProbeBuilder.GeometryValue |
MAXIMUM |
static ResultProbeBuilder.GeometryValue |
MINIMUM |
static ResultProbeBuilder.GeometryValue |
NONE |
static ResultProbeBuilder.GeometryValue |
SUM |
static ResultProbeBuilder.GeometryValue |
WEIGHTED_AVERAGE |
Modifier and Type | Method and Description |
---|---|
static ResultProbeBuilder.GeometryValue |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResultProbeBuilder.GeometryValue |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResultProbeBuilder.GeometryValue[] |
values()
Returns an array that contains the values for this enum.
|
public static final ResultProbeBuilder.GeometryValue ARITHMETIC_MEAN
public static final ResultProbeBuilder.GeometryValue MINIMUM
public static final ResultProbeBuilder.GeometryValue MAXIMUM
public static final ResultProbeBuilder.GeometryValue SUM
public static final ResultProbeBuilder.GeometryValue WEIGHTED_AVERAGE
public static final ResultProbeBuilder.GeometryValue INTEGRAL
public static final ResultProbeBuilder.GeometryValue NONE
public static final int _ARITHMETIC_MEAN
public static final int _MINIMUM
public static final int _MAXIMUM
public static final int _SUM
public static final int _WEIGHTED_AVERAGE
public static final int _INTEGRAL
public static final int _NONE
public static ResultProbeBuilder.GeometryValue valueOf(int value)
public static ResultProbeBuilder.GeometryValue valueOf(String name)
public static ResultProbeBuilder.GeometryValue[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.