public static class ProjectNodesToCadGeometryBuilder.ListingOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALL
List All information on nodes that are off the CAD geometry by more than the input tolerance
|
static int |
_NONE
List nothing
|
static int |
_SUMMARY_ONLY
List only Summary information
|
static ProjectNodesToCadGeometryBuilder.ListingOption |
ALL
List All information on nodes that are off the CAD geometry by more than the input tolerance
|
static ProjectNodesToCadGeometryBuilder.ListingOption |
NONE
List nothing
|
static ProjectNodesToCadGeometryBuilder.ListingOption |
SUMMARY_ONLY
List only Summary information
|
Modifier and Type | Method and Description |
---|---|
static ProjectNodesToCadGeometryBuilder.ListingOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProjectNodesToCadGeometryBuilder.ListingOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProjectNodesToCadGeometryBuilder.ListingOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final ProjectNodesToCadGeometryBuilder.ListingOption NONE
public static final ProjectNodesToCadGeometryBuilder.ListingOption SUMMARY_ONLY
public static final ProjectNodesToCadGeometryBuilder.ListingOption ALL
public static final int _NONE
public static final int _SUMMARY_ONLY
public static final int _ALL
public static ProjectNodesToCadGeometryBuilder.ListingOption valueOf(int value)
public static ProjectNodesToCadGeometryBuilder.ListingOption valueOf(String name)
public static ProjectNodesToCadGeometryBuilder.ListingOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.