public static class PreTestSensorConfigBuilder.AlgorithmChoiceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MIN_MAC |
static PreTestSensorConfigBuilder.AlgorithmChoiceType |
MIN_MAC |
Modifier and Type | Method and Description |
---|---|
static PreTestSensorConfigBuilder.AlgorithmChoiceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PreTestSensorConfigBuilder.AlgorithmChoiceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PreTestSensorConfigBuilder.AlgorithmChoiceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PreTestSensorConfigBuilder.AlgorithmChoiceType MIN_MAC
public static final int _MIN_MAC
public static PreTestSensorConfigBuilder.AlgorithmChoiceType valueOf(int value)
public static PreTestSensorConfigBuilder.AlgorithmChoiceType valueOf(String name)
public static PreTestSensorConfigBuilder.AlgorithmChoiceType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.