public interface PostScenarioSelectionParameters extends TaggedObject
PostScenarioInputDefinition
,
Data Source PostScenarioDataDefinition
, and PostScenarioVisualizationDefinition
. See PostScenarioBuilder
.
An instance can be created from a CAE.PostScenarioBuilder.
A valid user selection binds at least one value to each PostScenarioVariable
. The exact
constraints on the number of selected values varies which each scenario.
In order to bind values to variables, one must access each Variable from the
PostScenarioVariableCollection
, and bind values from those which are listed by the
Variable's PostScenarioVariable.getValues()
method.
PostScenarioConfigurationVariable
s are Scenario specific and enable or configure
scenario specific behaviour.
Modifier and Type | Method and Description |
---|---|
PostScenarioConfigurationVariableCollection |
configurationVariables()
Contains
PostScenarioConfigurationVariable s for this selection. |
PostScenarioVariant |
newVariant()
Create a new
PostScenarioVariant that wraps a scalar value. |
PostScenarioVariableCollection |
variables()
Contains selection
PostScenarioVariable s that define this selection. |
printTestData, printTestData, tag, tagValue
PostScenarioVariableCollection variables() throws RemoteException
RemoteException
PostScenarioConfigurationVariableCollection configurationVariables() throws RemoteException
RemoteException
PostScenarioVariant newVariant() throws NXException, RemoteException
PostScenarioVariant
that wraps a scalar value. These objects need to be Dispose'd of once it is no longer needed.
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.